24-bit DS A/D converter with programmable gain instrumentation amplifier
Below is a list of API functions output by the Code Generator for 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier use.
Table 3.21 API Functions: [24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.  | |
| 
       Performs user-defined initialization relating to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.  | |
| 
       Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.  | |
| 
       Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.  | |
| 
       Starts A/D conversion.  | |
| 
       Ends A/D conversion.  | |
| 
       Halts the clock supplied to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.  | |
| 
       Reads the results of A/D conversion.(mean value)  | |
| 
       Reads the results of A/D conversion.  | |
| 
       Connects the configurable amplifier to the 24-bit ΔΣ A/D converter and trims the offset.  | |
| 
       Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.  | |
| 
       Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.  |