Timer RD
Below is a list of API functions output by the Code Generator for timer RD use.
Table 3.7 API Functions: [Timer RD]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 16-bit timer RDn.  | |
| 
       Performs user-defined initialization relating to the 16-bit timer RDn.  | |
| 
       Performs processing in response to the timer interrupt.  | |
| 
       Starts the count for 16-bit timer RDn.  | |
| 
       Ends the count for 16-bit timer RDn.  | |
| 
       Halts the clock supplied to the 16-bit timer RDn.  | |
| 
       Starts the pulse output forced cutoff for 16-bit timer RDn,  | |
| 
       Ends the pulse output forced cutoff for 16-bit timer RDn.  | |
| 
       Reads the pulse width of the 16-bit timer RDn.  | |
| 
       Performs initialization necessary to control the 16-bit timer RDn.  | |
| 
       Performs user-defined initialization relating to the 16-bit timer RDn.  | |
| 
       Performs processing in response to the timer interrupt.  | |
| 
       Starts the count for 16-bit timer RDn.  | |
| 
       Ends the count for 16-bit timer RDn.  | |
| 
       Halts the clock supplied to the 16-bit timer RDn.  | |
| 
       Starts the pulse output forced cutoff for 16-bit timer RDn,  | |
| 
       Ends the pulse output forced cutoff for 16-bit timer RDn.  | |
| 
       Reads the pulse width of the 16-bit timer RDn.  | |
| 
       Halts the clock supplied to the 16-bit timer RD.  |