|
debugger.Timer.Information
|
This function displays conditional timer information.
[Specification format]
debugger.Timer.Information()
|
[Argument(s)]
None
[Return value]
List of conditional timer event information (see the TimerEventInfo class for detail)
[Detailed description]
- | This function displays conditional timer information displays in the following format. |
timer-event-number timer-name state start-address - end-address
|
[Example of use]
>>>ti = debugger.Timer.Information()
1 PythonTimer0001 Enable main - sub
>>>print ti[0].Number
1
>>>print ti[0].Name
PythonTimer0001
>>>
|