|
debugger.Assemble.Disassemble
|
This function performs disassembly.
[Specification format]
debugger.Assemble.Disassemble(address, number = 1, code = True)
|
[Argument(s)]
|
|
|
|
address
|
Specify the address at which to start disassembly.
|
|
number
|
Specify the number of lines to display (default: 1).
|
|
code
|
Specify whether to display instruction codes.
True: Display instruction codes (default).
False: Do not display instruction codes.
|
[Return value]
List of result of disassembly (see the DisassembleInfo property for detail)
[Detailed description]
- | This function performs disassembly from the address specified by address. |
- | If number is specified, the specified number of lines are displayed. |
- | If code is set to "False", then instruction codes are not displayed. |
- | If "." is specified in address, then it is interpreted as the address following the last address disassembled. |
[Example of use]
>>>debugger.Assemble.Disassemble("main")
0x00004088 F545 br _TestInit+0x8e
>>>debugger.Assemble.Disassemble("main", 2)
0x00004088 F545 br _TestInit+0x8e
0x0000408A 0A5A mov 0xa, r11
>>>debugger.Assemble.Disassemble("main", 5, False)
0x00004088 br _TestInit+0x8e
0x0000408A mov 0xa, r11
0x0000408C movea 0x19, r0, r13
0x00004090 mov r13, r12
0x00004092 movhi 0xffff, gp, r1
>>>
|