This function saves the memory data in Intel format.
[Specification format]
debugger.Upload.Intel(fileName, address1, address2, force = False)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify a file name.
|
|
address1
|
Specify an upload start address.
|
|
address2
|
Specify an upload end address.
|
|
force
|
Specify whether to overwrite.
True: Overwrite
False: Do not overwrite (default).
|
[Return value]
If the memory data was uploaded successfully: True
If there was an error when uploading the memory data: False
[Detailed description]
- | This function saves the memory data from address1 to address2 in Intel format. |
[Example of use]
>>>debugger.Upload.Intel("C:/test/testIntel.hex", 0x1000, 0x2000, True)
True
>>>
|