|
debugger.Download.LoadModule
|
This function downloads a load module.
[Specification format]
debugger.Download.LoadModule(fileName = "", downloadOption = DownloadOption.Both, append = False, flashErase = False, vendorType = VendorType.Auto)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify a download file.
|
|
downloadOption
|
Specify an option.
The options that can be specified are shown below.
|
|
|
|
|
DownloadOption.NoSymbol
|
Do not load symbol information.
|
|
DownloadOption.SymbolOnly
|
Only load symbol information.
|
|
DownloadOption.Both
|
Load both symbol information and object information (default).
|
|
append
|
Specify whether to make an additional download.
True: Perform additional download.
False: Perform overwrite download (default).
|
|
flashErase
|
Specify whether to initialize a flash memory before download.
True: Initialize a flash memory before download.
False: Do not initialize a flash memory before download (default).
|
|
vendorType
|
Specify the vendor of the compiler.
The types that can be specified are shown below.
|
|
|
|
|
VendorType.Auto
|
Automatically specify the vendor of the compiler judging from the output contents of debugging information (default).
|
|
VendorType.Ghs
|
Make this specification when using a compiler made by Green Hills Software, Inc.
|
[Return value]
If a binary file was downloaded successfully: True
If there was an error when downloading a binary file: False
[Detailed description]
- | This function downloads a load module. |
- | If fileName is not specified, the file specified on the [Download File Settings] tab in the Property panel of the debugging tool is downloaded. |
- | If downloadOption is specified, the processing is performed in accordance with the specification. |
[Example of use]
>>>debugger.Download.LoadModule("C:/test/testModule.lmf")
True
>>>debugger.Download.LoadModule("C:/test/testModule2.lmf", DownloadOption.SymbolOnly, True)
False
>>>
|