This function dumps the trace data.
[Specification format]
debugger.Trace.Get(frameCount, fileName = "", append = False)
|
[Argument(s)]
|
|
|
|
frameCount
|
Specify the number of dumps.
|
|
fileName
|
Specify the name of the file to dump to (default: not specified).
|
|
append
|
Specify whether to append trace data to the file.
True: Append trace data to the file.
False: Do not append trace data to the file (default).
|
[Return value]
List of trace information (see the TraceInfo property for detail)
[Detailed description]
- | This function dumps trace data for the number of frames specified by frameCount. |
- | If fileName is specified, then the trace data is written to the file. |
- | If append is set to "True", then the trace data is appended to the file. |
- | This function displays the trace data in the following format. Information which is not included in the trace data is displayed as blank space. |
For a single-core microcontroller
- | Execution of instructions |
number-of-frames timestamp fetch-address mnemonic
|
number-of-frames timestamp read-address R read-data
|
number-of-frames timestamp write-address W write-data
|
number-of-frames timestamp vector-read-address V vector-read-data
|
number-of-frames timestamp DMA
|
For a multi-core microcontroller
- | Execution of instructions |
number-of-frames PE-number timestamp fetch-address mnemonic
|
number-of-frames timestamp read-address R read-data
|
number-of-frames timestamp write-address W write-data
|
number-of-frames timestamp vector-read-address V vector-read-data
|
number-of-frames timestamp DMA
|
[Example of use]
>>>debugger.Trace.Get(3)
1851 00h00min00s003ms696μs000ns 0x000003be cmp r11, r14
1852 00h00min00s003ms700μs000ns 0x000003c0 blt _func_static3+0x2c
1853 00h00min00s003ms702μs000ns 0x000003c2 jarl _errfunc, lp
>>>debugger.XTrace.Dump(10, "C:/test/TestTrace.txt")
>>>
|