Everything

remainder / remainderf / remainderl


浮動小数点数同士の剰余を計算します。

[指定形式]

#include <math.h>

double remainder(double d1, double d2);

float remainderf(float d1, float d2);

long double remainderl(long double d1, long double d2);

[引数]

d1, d2 剰余を求める値 ( d1 / d2 )

[戻り値]

d1とd2の剰余値

[備考]

remainder関数群の剰余計算はIEEE 60559の規定に沿っています。