Everything

build.Library.EnableMathfH


アクティブ・プロジェクトのライブラリ・ジェネレート・オプションである,mathf.h(C89/C99)を有効にするかどうかの設定/参照を行います。【CC-RX】

[指定形式]

build.Library.EnableMathfH = bool

[設定]

設定

説明

bool

mathf.h(C89/C99)を有効にするかどうかを設定します。

True :mathf.h(C89/C99)とランタイムライブラリを有効にします。

False :mathf.h(C89/C99)を無効にします。

[参照]

mathf.h(C89/C99)とランタイムライブラリを有効にする場合 : True

mathf.h(C89/C99)を無効にする場合 : False

[詳細説明]

-

アクティブ・プロジェクトのライブラリ・ジェネレート・オプションである,mathf.h(C89/C99)を有効にするかどうかの設定/参照を行います。

[使用例]

>>>build.Library.EnableMathfH = True
>>>print build.Library.EnableMathfH
True
>>>