Property panel


This panel is used to display the detailed information on the analysis tool and change the settings of the information.

Figure A.3

Property Panel

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, select the [Program Analyzer (Analyze Tool)] node, and then select [Property] from the [View] menu.

-

On the Project Tree panel, select the [Program Analyzer (Analyze Tool)] node, and then select [Property] from the context menu.

Remark

If the Property panel has been opened, the detailed information on the analysis tool is displayed by selecting the [Program Analyzer (Analyze Tool)] node on the Project Tree panel.

[Description of each area]

(1)

Detailed information display/change area

In this area, the detailed information on the analysis tool is displayed by category in the list. Also, you can directly change its settings.

The mark indicates all the items in the category are expanded. The mark indicates all the items are shrink. You can expand/shrink the items by clicking these marks or double-clicking the category name.

For details on the information/how to setup in the category and property items contained in it, see the section explaining the corresponding tab.

(2)

Tab selection area

Categories for the display of the detailed information are changed when each tab is selected.

In this panel, a following tab is contained (see the section explaining the tab for details on the display/setting).

[[Edit] menu (Property panel-dedicated items)]

The [Edit] menu for this panel provides the following items and functions.

Undo

Undoes the latest property value editing being done.

Cut

Deletes the selected character string(s) and copies them to the clipboard while editing the property value.

Copy

Copies the contents of the selected range to the clipboard as character string(s).

Paste

Pastes the contents of the clipboard to the property value while editing the property value.

Delete

Deletes the selected character string(s) while editing the property value.

Select All

Selects all the character strings in the selected property while editing the property value.

[Context menu]

The context menu displayed by right-clicking on this panel provides the following items and functions.

(1)

While not editing the property value

Reset to Default

Restores the selected setting of the property item to default value.

Reset All to Default

Restores all the selected settings of the property items on the tab to default value.

(2)

While editing the property value

Undo

Undoes the latest property value editing being done.

Cut

Deletes the selected character string(s) and copies them to the clipboard while editing the property value.

Copy

Copies the contents of the selected range to the clipboard as character string(s).

Paste

Pastes the contents of the clipboard to the property value while editing the property value.

Delete

Deletes the selected character string(s) while editing the property value.

Select All

Selects all the character strings in the selected property while editing the property value.