3.2.3 Port functions

Below is a list of API functions output by the Code Generator for port functions use.

Table 3.3

API Functions: [Port Functions]

API Function Name

Function

R_PORT_Create

Performs initialization necessary to control the port functions.

R_PORT_Create_UserInit

Performs user-defined initialization relating to the port functions.