divf.s


Floating-point division (single precision) (Floating-point Divide (Single))

[Syntax]

-

divf.s reg1, reg2, reg3

[Function]

This instruction divides the single-precision floating-point format contents of general-purpose register reg2 by the single-precision floating-point format contents of general-purpose register reg1, and stores the result in general-purpose register reg3. The operation is executed as if it were of infinite accuracy, and the result is rounded in accordance with the current rounding mode.

[Description]

-

The assembler generates one divf.s machine instruction.