Conversion to floating-point format (double precision) (Floating-point Convert Unsigned-Long to Double (Double))
This instruction arithmetically converts the unsigned 64-bit fixed-point format contents of the register pair specified by general-purpose register reg1 to double-precision floating-point format in accordance with the current rounding mode, and stores the result in the register pair specified by general-purpose register reg2.