Memory Search dialog box


This dialog box searches for memory values. (See "2.11.1.5 Searching for memory contents")

A search is performed in either the Memory value area or Character string area in which the caret on the Memory panel was present immediately before this dialog box is opened.

Figure A.54

Memory Search Dialog Box

 

Here, the following items are explained.

[How to open]

-

Choose [Find...] from the context menu on Memory panel.

[Description of each area]

(1)

[Search Data] area

Specify the data to search.

Enter directly in the text box (specifiable in up to 256 bytes) or select an input history item from the drop-down list (up to 10 history entries).

If the subject of search is in the Memory value area of the Memory panel, the data needs to be entered in the same form (numeral system and size) as displayed in that area.

Also, the subject of search is in the Character string area, it is necessary to specify a character string as the data to search. The specified character string, before being searched, is converted to data in appropriate encoding form in which data are displayed in that area.

Note that if any memory value was selected immediately before this dialog box was opened, then the selected value is displayed by default.

(2)

[Search Range] area

Select a range in which to search from the drop-down list below.

Specify address range

A search is conducted within the address range specified by [Address] area.

Memory mapping

A search is conducted within the selected range of memory mapping.

This list item displays memory mappings individually (except non-mapped areas) that are displayed in the Memory Mapping dialog box.

Display form: <Memory type> <Address range> <Size>

(3)

[Address] area

This item is valid only when [Specify Address Range] is selected in the [Search Range] area.

Specify the "start address" and "end address" to set the address range in which a memory value is searched. Directly enter address expressions in the respective text boxes (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).

The calculation results of the entered address expressions are handled respectively as the start address and end address.

However, searchable addresses are limited to the upper-limit address of the program space (0xFFFFFFFF).

Also, no address values can be specified that are greater than the value representable by 32 bits.

Remark 1.

By holding down [Ctrl]+[Space] keys in this text box, you can complete the symbol name at the present caret position (see "2.21.2 Symbol name completion function").

Remark 2.

If the "start address" text box is blank, address "0x0" is assumed.

Remark 3.

If the "end address" text box is blank, the upper-limit address of the microcontroller's address space is assumed.

[Function buttons]

Button

Function

Search Backward

Performs a search in the direction toward smaller addresses within the range specified in the [Search Range] area and [Address] area. The searched spot is placed in selected state on Memory panel.

However, if an invalid value is specified, or when the program is under execution, a message is displayed and a search for memory value is not performed.

Also, if the Memory panel is hidden, or if focus is moved to this dialog box while focus was present on another panel, this button is disabled.

Search Forward

Performs a search in the direction toward larger addresses within the range specified in the [Search Range] area and [Address] area. The searched spot is placed in selected state on Memory panel.

However, if an invalid value is specified, or when the program is under execution, a message is displayed and a search for memory value is not performed.

Also, if the Memory panel is hidden, or if focus is moved to this dialog box while focus was present on another panel, this button is disabled.

Cancel

Nullifies settings for a search of memory value and closes this dialog box.

Help

Displays help for this dialog box.