Current Consumption Measurement Trigger Condition Setting dialog box [E2] |
This dialog box is used to set trigger conditions in the Measuring Current Consumption panel [E2].
This section describes the following.
On the Measuring Current Consumption panel [E2], click the |
Specify whether to use the trigger function.
Set the operation of the E2 emulator on detection of the trigger.
Select the operation on detection of the trigger from the following drop-down list.
Output the external trigger signal by using the function for output of an external trigger signal from the extended interface of the E2 emulator. |
When "Output external trigger signal" is selected for [Action when detecting a trigger], select "ch0" or "ch1" as the external trigger output channel of the extended interface of the E2 emulator.
Select [High pulse] or [Hold High level during the current meets the condition] as the type of signal for output as the external trigger.
When [High pulse] is selected, specify the width of the pulse as a decimal value between 1 and 65535 (in microseconds).
Select the type of change in values for current as the trigger condition from the following drop-down list.
Specify the specific value or range of values for current to serve as the trigger condition in microamperes.
Specify one value for current when "Over threshold" or "Under Threshold" is selected for [Condition], and two values for current when "In range" or "Out of Range" is selected for [Condition].
For a range of current values, the value entered in the left field for entry must be lower than that in the right field. |
When "Over threshold", "Under Threshold", or "In range" is selected for [Condition], specify whether the trigger is only detected when the change in the value for current continues for a specific period or at the instant the required change in the value is detected.
To select detection of the trigger, select the check box and specify the condition for the interval and the interval.
Select the condition for the interval from the following drop-down list.
Specify a multiple of the sampling time selected for [Sampling time] in the Current Consumption Measurement Condition Setting dialog box [E2].
The actual interval is the specified multiple of the sampling time.
Reflects the settings of the trigger conditions that were made in this dialog box to the Measuring Current Consumption panel [E2]. |
|