2.23.18 Coverage measurement function [E20 [RX71M, RX64M, RX651, RX65N]]

When the processing after an interrupt does not return execution to the processing where the interrupt occurred, the next or second unexecuted instruction after the interrupt occurrence location is displayed as an executed instruction.