The external trace output and real-time RAM monitor functions via FINE interface are not supported. |
[RX62x, RX630, RX631, RX63N, RX63T, RX634]
The FINE interface supports only a two-wire system making use of FINEC and MD/FINED pins. One-wire systems are not supported. |
[RX71M, RX651, RX65N, RX64M, RX210, RX21A, RX220, RX23x, RX24T, RX110, RX111, RX113, RX130]