In debugging that includes rewriting of the flash memory, issuing a pin reset or an internal reset during execution of the program may prevent updating of the display in the Disassemble panel or Memory panel.
In such cases, manually operate the ROM cache invalidate register (ROMCIV) and disable the ROM cache after the user program has stopped.