2.23.8 DMAC and DTC

When either of the following conditions is met or when both of them are met,

-

An address in the microcontroller's on-chip flash ROM is specified as the origin of a DMAC or DTC transfer

-

An address in the microcontroller's on-chip flash ROM is specified as the interrupt vector for a DMAC or DTC activation source or the DTC vector table

 

do not perform any of the following operations if a DMAC or DTC request may be generated while the user program is stopped.

-

Setting a software breakpoint in the microcontroller's internal flash ROM area

-

Writing to the microcontroller's internal flash ROM area from the Memory panel or Python console panel

-

Downloading to the microcontroller's internal flash ROM area