Reads the alarm conditions (weekday, hour, minute).(in the case of the binary mode setting)
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_rtc.h
void R_RTC_Get_BinaryAlarmValue ( uint32_t * const alarm_enable,
uint32_t * const alarm_val );
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 O  | 
 uint32_t * const alarm_enable;  | 
 Pointer to structure in which to store the alarm enable value being read  | 
| 
 O  | 
 uint32_t * const alarm_val;  | 
 Pointer to structure in which to store the conditions being read  | 
[Return value]
None.