R_RTC_Set_BinaryCounterValue

Sets the counter value of the real-time clock.(in the case of the binary mode setting)

[Syntax]

#include r_cg_macrodriver.h

#include r_cg_rtc.h

MD_STATUS R_RTC_Set_BinaryCounterValue ( uint32_t counter_write_val );

[Argument(s)]

I/O

Argument

Description

I

uint32_t counter_write_val;

Counter value

[Return value]

Macro

Description

MD_OK

Normal completion

MD_BUSY1

Executing count process (before change to setting)

Remark If MD_BUSY1 is returned, it may be because the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger.