R_RTC_Get_BinaryCounterValue

Reads the counter value of the real-time clock.(in the case of the calendar mode setting)

[Syntax]

#include r_cg_macrodriver.h

#include r_cg_rtc.h

MD_STATUS R_RTC_Get_BinaryCounterValue ( uint32_t * const counter_read_val );

[Argument(s)]

I/O

Argument

Description

O

uint32_t * const counter_read_val;

Pointer to structure in which to store the counter value being read

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR

Read failure