r_rtc_periodinterrupt

Performs processing in response to the periodic interrupt INTRTCPRD.

Remark This API function is called as the interrupt process corresponding to the periodic interrupt INTRTCPRD.

[Syntax]

CA78K0R Compiler

__interrupt static void r_rtc_periodinterrupt ( void );

CC-RL Compiler

static void __near r_rtc_periodinterrupt ( void );

[Argument(s)]

None.

[Return value]

None.