Starts the alarm interrupt function.(in the case of the calendar mode setting)
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_rtc.h
void R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set );
[Argument(s)]
| 
 I/O  | 
 Argument  | 
 Description  | 
| 
 I  | 
 uint8_t enb_set;  | 
 Alarm enable  | 
Remark Below is shown the structure enb_set.
![]()  | 
[Return value]
None.