Generate an alarm intetrrupt every 10 minutes between AM7:00 and AM7:59.
[GUI setting example]
| 
 Real-time clock  | 
 Used  | |||
| 
 RTC  | 
 Used  | |||
| 
 Real-time clock operation setting  | 
 Used  | |||
| 
 Hour-system selection  | 
 24-hour  | |||
| 
 Set real-time clock initial value  | 
 Used 04/01/2018 00:00:00  | |||
| 
 Enable output of RTC1HZ pin (1 Hz)  | 
 Unused  | |||
| 
 Use alarm detection function  | 
 Used  | |||
| 
 Set alarm initial value  | 
 Used  | |||
| 
 Week day  | 
 Sunday Monday Tuesday Wednesday Thursday Friday Saturday  | |||
| 
 Hour: Minute  | 
 AM 07:00  | |||
| 
 Used as alarm interrupt function (INTRTC)  | 
 Used  | |||
| 
 Used as condtant-period interrupt function (INTRTC)  | 
 Unused  | |||
| 
 Priority(INTRTC)  | 
 Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Enable the real-time clock */
R_RTC_Start();
/* Start the alarm operation */
R_RTC_Set_AlarmOn();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_rtc_user.c
/* Start user code for global. Do not edit comment generated here */
volatile rtc_alarm_value_t alarm_val;
/* End user code. Do not edit comment generated here */
static void r_rtc_callback_alarm(void)
{
/* Start user code. Do not edit comment generated here */
/* Get alarm value */
R_RTC_Get_AlarmValue((rtc_alarm_value_t *)&alarm_val);
if ((alarm_val.alarmwm + 0x10U) <= 0x59U)
{
alarm_val.alarmwm += 0x10U;
/* Set alarm value */
R_RTC_Set_AlarmValue(alarm_val);
}
else
{
/* Stop the alarm operation */
R_RTC_Set_AlarmOff();
}
/* End user code. Do not edit comment generated here */
}