32-bit Multiply-accumulator
Below is a list of API functions output by the Code Generator for 32-bit Multiply-accumulator use.
Table 3.48 API Functions: [32-bit Multiply-accumulator]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 32-bit Multiply-accumulator.  | |
| 
       Performs user-defined initialization relating to the 32-bit Multiply-accumulator.  | |
| 
       Performs processing in response to the 32-bit Multiply-accumulator interrupt INTMACLOF.  | |
| 
       Resets the 32-bit Multiply-accumulator.  | |
| 
       Stops the cock supplied for the 32-bit Multiply-accumulator.  | |
| 
       Operates the unsigned multiply.  | |
| 
       Operates the signed multiply.  | |
| 
       Operates the unsigned multiply-accumulate.  | |
| 
       Operates the signed multiply-accumulate.  |