DMA controller
Below is a list of API functions output by the Code Generator for DMA controller use.
Table 3.37 API Functions: [DMA Controller]
| API Function Name | Function | 
| Performs initialization necessary to control the DMA controller. | |
| Performs user-defined initialization relating to the DMA controller. | |
| Performs initialization necessary to control the DMA controller. | |
| Performs user-defined initialization relating to the DMA controller. | |
| Performs processing in response to the DMA transfer end interrupt INTDMAn. | |
| Enables operation of channel n. | |
| Disables operation of channel n. | |
| Starts DMA transfer. |