Serial array unit
Below is a list of API functions output by the Code Generator for serial array unit use.
Table 3.30 API Functions: [Serial Array Unit] (1)
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the serial array unit.  | |
| 
       Performs user-defined initialization related to the serial array unit.  | |
| 
       Reset the serial array unit.  | |
| 
       Halts the clock supplied to the serial array unit.  | |
| 
       Enables the switch from STOP mode to SNOOZE mode.  | |
| 
       Disables the switch from STOP mode to SNOOZE mode.  | |
| 
       Performs initialization necessary to perform the UART communication.  | |
| 
       Performs processing in response to the UART transmission end interrupt INTSTn.  | |
| 
       Performs processing in response to the UART reception end interrupt INTSRn.  | |
| 
       Performs processing in response to the reception error interrupt INTSREn.  | |
| 
       Sets UART communication to standby mode.  | |
| 
       Ends UART communication.  | |
| 
       Starts UART data transmission.  | |
| 
       Starts UART data reception.  | |
| 
       Performs processing in response to the UART transmission end interrupt INTSTn.  | |
| 
       Performs processing in response to the UART reception end interrupt INTSRn.  | |
| 
       Performs processing in response to the UART reception error interrupt INTSREn.  | |
| 
       Performs processing in response to detection of overrun error.  | |
| 
       Performs initialization necessary to perform the 3-wire serial I/O communication.  | |
| 
       Performs processing in response to the CSI communication end interrupt INTCSImn.  | |
| 
       Sets 3-wire serial I/O communication to standby mode.  | |
| 
       Ends 3-wire serial I/O communication.  | |
| 
       Starts CSI data transmission.  | |
| 
       Starts CSI data reception.  | |
| 
       Starts CSI data transmission/reception.  | |
| 
       Performs processing in response to the CSI transmission end interrupt INTCSImn.  | 
Table 3.31 API Functions: [Serial Array Unit] (2)
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs processing in response to the CSI reception end interrupt INTCSImn.  | |
| 
       Performs processing in response to the CSI reception error interrupt INTSREn.  | |
| 
       Performs initialization necessary to perform the simplified IIC communication.  | |
| 
       Performs processing in response to the simple IIC communication end interrupt INTIICmn.  | |
| 
       Generates start conditions.  | |
| 
       Generates stop conditions.  | |
| 
       Ends simplified IIC communication.  | |
| 
       Starts simple IIC master transmission.  | |
| 
       Starts simple IIC master reception.  | |
| 
       Performs processing in response to the simple IICmn master transmission end interrupt INTIICmn.  | |
| 
       Performs processing in response to the simple IICmn master reception end interrupt INTIICmn.  | |
| 
       Performs processing in response to detection of parity error (ACK error).  |