Common
Below is a list of API functions output by the Code Generator for common use.
Table 3.1 API Functions: [Common]
| API Function Name | Function | 
| Performs initialization necessary to control the various hardwares. This API is automatically called from the startup routine of Renesas-made compiler. | |
| Performs initialization necessary to control the various peripheral functions. | |
| This is a main function. | |
| Performs user-defined initialization. |