Interrupt functions
Below is a list of API functions output by the Code Generator for interrupt functions use.
Table 3.40 API Functions: [Interrupt Functions]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the interrupt functions.  | |
| 
       Performs user-defined initialization relating to the interrupt functions.  | |
| 
       Performs processing in response to the external maskable interrupt INTPn.  | |
| 
       Enables the acceptance of the external maskable interrupts INTPn.  | |
| 
       Disables the acceptance of the external maskable interrupts INTPn.  | |
| 
       Performs processing in response to the external maskable interrupt INTPLRn.  | |
| 
       Enables the acceptance of the external maskable interrupts INTPLRn.  | |
| 
       Disables the acceptance of the external maskable interrupts INTPLRn.  | |
| 
       Performs processing in response to the external maskable interrupt INTRTCICn.  | |
| 
       Enables the acceptance of the external maskable interrupts INTRTCICn.  | |
| 
       Disables the acceptance of the external maskable interrupts INTRTCICn.  | |
| 
       Enables the acceptance of the external maskable interrupts INTFO.  | |
| 
       Disables the acceptance of the external maskable interrupts INTFO.  | |
| 
       Clears INTFCLR flag of Interrupt flag output control register 1 (INTFOCTL1).  | |
| 
       Performs processing in response to the external maskable interrupt INTFO.  |