Timer array unit
Below is a list of API functions output by the Code Generator for timer array unit use.
Table 3.5 API Functions: [Timer Array Unit]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the timer array unit.  | |
| 
       Performs user-defined initialization relating to the timer array unit.  | |
| 
       Performs processing in response to the timer interrupt INTTMmn.  | |
| 
       Performs processing in response to the timer interrupt INTTMmnH.  | |
| 
       Starts the count for channel n.  | |
| 
       Starts the count (higher 8-bit) for channel n.  | |
| 
       Starts the count (lower 8-bit) for channel n.  | |
| 
       Ends the count for channel n.  | |
| 
       Ends the count (higher 8-bit) for channel n.  | |
| 
       Ends the count (lower 8-bit) for channel n.  | |
| 
       Reset the timer array unit.  | |
| 
       Halts the clock supplied to the timer array unit.  | |
| 
       Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin.  | |
| 
       Generates the trigger (software trigger) for one-shot pulse output.  |