Performs processing in response to the CSI reception error interrupt INTSREn.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_error corresponding to the CSI reception error interrupt INTSREn.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_csimn_callback_error ( uint8_t err_type );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
uint8_t err_type; |
Trigger for CSI reception error interrupt 00000xx1B: Overrun error |
[Return value]
None.