Everything

r_uartn_callback_softwareoverrun

Performs processing in response to detection of overrun error.

Remark         This API function is called as the callback routine of interrupt process r_uartn_interrupt_receive corresponding to the UART reception end interrupt INTSRn (process performed when the amount of data received is greater than the argument rx_num specified for R_UARTn_Receive ).

 

[Syntax]

#include    “r_cg_macrodriver.h”

static void   r_uartn_callback_softwareoverrun ( uint16_t rx_data );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

O

uint16_t rx_data;

Receive data (greater than the argument rx_num specified for R_UARTn_Receive)

 

[Return value]

None.