Performs processing in response to the UART reception end interrupt INTSRn.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_receive corresponding to the UART transmission end interrupt INTSRn (performed when number of received data specified by R_UARTn_Receive argument rx_num has been completed).
[Syntax]
static void r_uartn_callback_receiveend ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.