Everything

r_csimn_interrupt

Performs processing in response to the CSI communication end interrupt INTCSImn.

Remark         This API function is called as the interrupt process corresponding to the CSI communication end interrupt INTCSImn.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_csimn_interrupt ( void );

 

CC-RL Compiler

static void   __near r_csimn_interrupt ( void );

Remark         m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.