Performs processing in response to the CSI reception end interrupt INTCSImn.
Remark This API function is called as the callback routine of interrupt process r_csimn_interrupt corresponding to the CSI reception end interrupt INTCSImn (performed when number of received data specified by R_CSImn_Receive or R_CSImn_Send_Receive argument rx_num has been completed).
[Syntax]
static void r_csin_callback_receiveend ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]
None.