Performs processing in response to the simple IICmn master transmission end interrupt INTIICmn.
Remark This API function is called as the callback routine of interrupt process r_iicmn_interrupt corresponding to the simple IICmn master transmission end interrupt INTIICmn (performed when number of transmission data specified by R_IICmn_Master_Send argument tx_num has been completed).
[Syntax]
static void r_iicmn_callback_master_sendend ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]
None.