Enables batch overwriting of the compare register.
Remark The timing for batch-overwriting the content of the compare register is when a count value and a value set in the compare register are matched or an external trigger is generated after calling this API function.
[Syntax]
void R_KB2m_BatchOverwritRequestOn ( void );
Remark m is the unit number.
[Argument(s)]
None.
[Return value]
None.