R_KB2m_TKBOn0_SmoothStartFunction_Stop
Ends smooth start function for timer
output TKBOn0.
[Syntax]
void
R_KB2m_TKBOn0_SmoothStartFunction_Stop ( void );
Remark
m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return
value]
None.