R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Stop
Ends forced output stop function 2 for
timer output TKBOn1.
[Syntax]
void
R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Stop ( void
);
Remark
m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return
value]
None.