Starts dithering function for timer output TKBOn0.
[Syntax]
void R_KB2m_TKBOn0_DitheringFunction_Start ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]