R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start
Starts forced output stop function 2
for timer output TKBOn1.
[Syntax]
void
R_KB2m_TKBOn1_Forced_Ourput_Stop_Function1_Start ( void
);
Remark
m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return
value]
None.