Everything

16-bit timer KB2

Below is a list of API functions output by the Code Generator for 16-bit timer KB2 use.

 

Table 3.12 API Functions: [16-bit Timer KB2]

API Function Name

Function

R_KB2m_Create

Performs initialization necessary to control the 16-bit timer KB2.

R_KB2m_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer KB2.

r_kb2m_interrupt

Performs processing in response to the timer interrupt INTTKB2m.

R_KB2m_Start

Starts the count for 16-bit timer KB2.

R_KB2m_Stop

Ends the count for 16-bit timer KB2.

R_KB2m_Set_PowerOff

Halts the clock supplied to the 16-bit timer KB2.

R_KB2m_Simultaneous_Start

Starts the simultaneous start/stop mode.

R_KB2m_Simultaneous_Stop

Ends the simultaneous start/stop mode.

R_KB2m_Synchronous_Start

Starts the timer start/clear mode.

R_KB2m_Synchronous_Stop

Ends the timer start/clear mode.

R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Start

Starts forced output stop function 1 for timer output TKBOn0.

R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop

Ends forced output stop function 1 for timer output TKBOn0.

R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start

Starts forced output stop function 2 for timer output TKBOn1.

R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Stop

Starts forced output stop function 2 for timer output TKBOn1.

R_KB2m_TKBOn0_DitheringFunction_Start

Starts dithering function for timer output TKBOn0.

R_KB2m_TKBOn0_DitheringFunction_Stop

Ends dithering function for timer output TKBOn0.

R_KB2m_TKBOn1_DitheringFunction_Start

Starts dithering function for timer output TKBOn1.

R_KB2m_TKBOn1_DitheringFunction_Stop

Ends dithering function for timer output TKBOn1.

R_KB2m_TKBOn0_SmoothStartFunction_Start

Starts smooth start function for timer output TKBOn0.

R_KB2m_TKBOn0_SmoothStartFunction_Stop

Ends smooth start function for timer output TKBOn0.

R_KB2m_TKBOn1_SmoothStartFunction_Start

Starts smooth start function for timer output TKBOn1.

R_KB2m_TKBOn1_SmoothStartFunction_Stop

Ends smooth start function for timer output TKBOn1.

R_KB2m_BatchOverwriteRequestOn

Enables batch overwriting of the compare register.