Everything

R_RTC_Get_BinaryAlarmValue

Reads the alarm conditions (weekday, hour, minute).(in the case of the binary mode setting)

 

[Syntax]

#include  “r_cg_macrodriver.h”

#include  “r_cg_rtc.h”

void       R_RTC_Get_BinaryAlarmValue ( uint32_t * const alarm_enable,

 uint32_t * const alarm_val );

 

[Argument(s)]

I/O

Argument

Description

O

uint32_t * const alarm_enable;

Pointer to structure in which to store the alarm enable value being read

O

uint32_t * const alarm_val;

Pointer to structure in which to store the conditions being read

 

[Return value]

None.