Everything

R_RTC_Set_CalendarAlarmOn

Starts the alarm interrupt function.(in the case of the calendar mode setting)

 

[Syntax]

#include  “r_cg_macrodriver.h”

#include  “r_cg_rtc.h”

void       R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set );

 

[Argument(s)]

I/O

Argument

Description

I

uint8_t enb_set;

Alarm enable

Remark         Below is shown the structure enb_set.

 

 

 

 

 

 

 

 

 

 

 

 


[Return value]

None.