Everything

R_RTC_Set_PowerOff

Halts the clock supplied to the real-time clock.

Remark 1.      Calling this API function changes the real-time clock to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

Remark 2.      This API function stops the clock supply to the real-time clock, by operating the RTCEN bit of peripheral enable register n.
For this reason, this API function also stops the clock supply to other peripheral devices sharing the RTCEN bit (e.g. interval timer).

 

[Syntax]

void       R_RTC_Set_PowerOff ( void );

 

[Argument(s)]

None.

 

[Return value]

None.