Reads the counter value of the real-time clock.(in the case of the calendar mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
MD_STATUS R_RTC_Get_CalendarCounterValue ( rtc_counter_value_t * const counter_read_val );
[Argument(s)]
I/O |
Argument |
Description |
O |
rtc_counter_value_t * const counter_read_val; |
Pointer to structure in which to store the counter value being read |
Remark See R_RTC_Set_CounterValue for details about the rtc_counter_value_t counter value.
[Return value]
Macro |
Description |
MD_OK |
Normal completion |
MD_ERROR |
Read failure |