Everything

R_RTC_Get_CalenderAlarmValue

Reads the alarm conditions (year, month, weekday, day, hour, minute, second).(in the case of the calendar mode setting)

 

[Syntax]

#include  “r_cg_macrodriver.h”

#include  “r_cg_rtc.h”

void       R_RTC_Get_CalenderAlarmValue ( rtc_alarm_value_t * const alarm_val );

 

[Argument(s)]

I/O

Argument

Description

O

rtc_alarm_value_t * const alarm_val;

Pointer to structure in which to store the conditions being read

Remark         See R_RTC_Set_AlarmValue for details about rtc_alarm_value_t (alarm conditions).

 

[Return value]

None.