Everything

R_RTC_Set_BinaryAlarmValue

Sets the alarm conditions.(in the case of the binary mode setting)

 

[Syntax]

#include  “r_cg_macrodriver.h”

#include  “r_cg_rtc.h”

void       R_RTC_Set_BinaryAlarmValue ( uint32_t alarm_enable, uint32_t alarm_val );

 

[Argument(s)]

I/O

Argument

Description

I

uint32_t alarm_enable;

Alarm enable
(Set the value to the Binary Counter Alarm Enable Register)

I

uint32_t alarm_val;

Alarm conditions (count value)

(Set the value to the Binary Counter Alarm Register)

 

[Return value]

None.