This dialog box is used to set the serial format for the serial interface (IICA).
This section describes the following.
On the Serial window with the IICA serial interface, any one of the following:
|
Directly inputs the width at high level of the serial clock. |
||
|
Directly inputs the address of the slave which is to be the other party. |
||
|
Selects this item to repeat data transfer when the [Auto Send] or [Auto Receive] button in the Serial window has been clicked. |
||
|
Following transmission of the last data during automatic transmission, returns to the beginning of the data and performs automatic transmission. Following reception of the last data during automatic reception, returns to the beginning of the Wait time and performs automatic reception. |
||
|
Following transmission of the last data during automatic transmission, stops transmission. Following reception of the last data during automatic reception, stops reception. |
||
|
Selects this item to repeat data transfer when the [Auto Send] or [Auto Receive] button in the Serial window has been clicked. |
||
|
Following transmission of the last data during automatic transmission, returns to the beginning of the data and performs automatic transmission. Following reception of the last data during automatic reception, returns to the beginning of the Wait time and performs automatic reception. |
||
|
Following transmission of the last data during automatic transmission, stops transmission. Following reception of the last data during automatic reception, stops reception. |
||
(default)
(default)